Locale Icon
English
EngineerZone
EngineerZone
Gigabit Multimedia Serial Link (GMSL) Library
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
    Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 2: Achieving Phase Repeatability

    This article discusses a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a...

Gigabit Multimedia Serial Link (GMSL) Library
  • Interface and Isolation
Gigabit Multimedia Serial Link (GMSL) Library
FAQs
  • FAQs
  • Documents
  • Members
  • Tags
  • Cancel
Browse Categories
  • GMSL1
  • GMSL2
  • GMSL U
  • Features
  • ChannelSpec
  • Documentation
  • EMI
  • Glossary
  • Hardware
  • MAX9205: FAQ
  • MAX9217: FAQ
  • MAX9271: FAQ
  • MAX9275: FAQ
  • MAX9276A: FAQ
  • MAX9277: FAQ
  • MAX9278: FAQ
  • MAX9281: FAQ
  • MAX9286: FAQ
  • MAX9288: FAQ
  • MAX9291: FAQ
  • MAX96705: FAQ
  • MAX96705A: FAQ
  • MAX96706: FAQ
  • MAX96707: FAQ
  • MAX96715: FAQ
  • Safety
  • Software
  • Training
  • Troubleshooting
Manage My Notifications
  • More
  • Cancel
  • FAQs

Documentation

GMSL Documentation

FAQs
  • FAQ

    Are there any blanking requirements from a GMSL point of view? Can we use 0 blanking? What is the blanking time that you recommend?

    There are blanking requirements stated in the data sheet, and zero blanking time is not supported. In general, CVT-RB timings are a good place to start for video timing proposals, then modified as needed…
  • FAQ

    My ESD test results are below the data sheet limit

    The limits given in the data sheet EC table are per ISO10605, RD = 330Ω, CS = 150pF for Contact and Air discharge and Human Body Model, RD = 1.5kΩ, CS = 100pF, with device powered off.
  • FAQ

    What are the forward and reverse channel latencies for I2C transactions sent across the GMSL Link?

    This latency can be approximated to the same values given for GPIO delay (without delay compensation). For forward channel it is about 1 μs and for reverse channel it is about 6 μs for GMSL2 use-case,…
  • FAQ

    What are the typical and maximum power consumption values given in GMSL part data sheets?

    Typical value of supply current is not a reference for power supply sizing, use the maximum supply value for reference. Typical value of supply current is an indicative value of current consumption which…
  • FAQ

    What is pixel clock and how is it calculated?

    The pixel clock is the clock rate of pixels in a video stream. The following equations can be used to calculate pixel clock: PCLK = Htotal * Vtotal * Framerate PCLK = (Active Width) * (Active Height)…
  • FAQ

    What is the difference in nomenclature between a local device and remote device?

    It's best to think of this terminology relative to the host processor. For cameras or sensors, the deserializer is connected to the processor so it is "local" and the serializer connected on the other…
  • FAQ

    Which ADC voltage reference should be used?

    For MAX96717 and MAX96717F, we recommend using 1.25V internal voltage reference. The setup of these voltage references, and ADC setup, can be found in the MAX96717 User Guide. Note: MAX96717R does not…