FAQ I am using a GMSL2 part in GMSL1 mode. which channel spec should I use?

Customers should follow the GMSL specification according to whichever mode is being used. thus a part working in GMSL1 mode should follow the GMSL1 specs. However, to reduce the amount of redesign, it is best to pass the specifications of all possible modes that a part is capable of, to allow for better reuse in the future. A board for the MAX96724, capable of GMSL2 and GMSL1 modes, should pass the 6G GMSL2, 3G GMSL2, and 3.125G GMSL1 specs.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.