Locale Icon
English
EngineerZone
EngineerZone
Gigabit Multimedia Serial Link (GMSL) Library
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
    Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    View All Webinars
  • Community Hub

    Challenge Yourself!

      New KCC Quiz AQQ299 about Opamp Open Loop Gain and LTspice

      A kind proposal from Al Butvidas 1. Quote of the month: " A good friend calls you in jail. A great friend bails you out of jail. Your best friend sits...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Master FPGA-Based DSP Design: The Complete Building Blocks Guide You Need to Read

    The Engineering Mind Blog on EngineerZone presents an exceptional five-part series titled " DSP Building Blocks " that walks engineers through the essential...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    PSM Integration for Enhanced Module Solutions in 48 V Data Centers

    The integration of the LTC2971 into quarter brick solutions for 48 V data centers enhances monitoring, control, and reliability by providing high precision...

Gigabit Multimedia Serial Link (GMSL) Library
  • Interface and Isolation
Gigabit Multimedia Serial Link (GMSL) Library
FAQs
  • FAQs
  • Documents
  • Members
  • Tags
  • Cancel
Browse Categories
  • GMSL1
  • GMSL2
  • GMSL U
  • Features
  • ChannelSpec
  • Documentation
  • EMI
  • Glossary
  • Hardware
  • MAX9205: FAQ
  • MAX9217: FAQ
  • MAX9271: FAQ
  • MAX9275: FAQ
  • MAX9276A: FAQ
  • MAX9277: FAQ
  • MAX9278: FAQ
  • MAX9281: FAQ
  • MAX9286: FAQ
  • MAX9288: FAQ
  • MAX9291: FAQ
  • MAX96705: FAQ
  • MAX96705A: FAQ
  • MAX96706: FAQ
  • MAX96707: FAQ
  • MAX96715: FAQ
  • Safety
  • Software
  • Training
  • Troubleshooting
Manage My Notifications
  • More
  • Cancel
  • FAQs

ChannelSpec

Channel Specification/ Signal Integrity

FAQs
  • FAQ

    How do I measure/decode the serial data (GMSL1)?

    GMSL1 has both forward and reverse data. A customer would need to use high impedance probes and use filtering to take out only the forward or reverse data. As GMSL is a proprietary link, there is not much…
  • FAQ

    How do I measure/decode the serial data (GMSL2)?

    GMSL2 has both forward and reverse data. Due to the proprietary nature of the GMSL link, a customer will not be able to see meaningful data. It is better to check for decode/PRBS/CRC errors.
  • FAQ

    How is Link Margin performed?

    Link margin testing is performed by reducing the peak-to-peak source voltage until an error has occurred.
  • FAQ

    How much insertion loss can a GMSL2 system tolerate?

    The allowable insertion loss depends on the selected bit rate and. It is given in the GMSL Channel Specification.
  • FAQ

    I am not building all sections of a GMSL channel. How do I determine I have a compliant channel?

    The Channel specs include specifications for 2 types of individual modules: The PCB channel and the cable channel.
  • FAQ

    I am passing the Link Margin test, but my system is failing the GMSL channel specification. Is my system compliant and expected to work?

    The expectation is that the cable and system never fail the GMSL channel specification limits. The cable or system, under all expected conditions, must still pass the channel specification. Link margin…
  • FAQ

    I am using a GMSL2 part in GMSL1 mode. which channel spec should I use?

    Customers should follow the GMSL specification according to whichever mode is being used. thus a part working in GMSL1 mode should follow the GMSL1 specs. However, to reduce the amount of redesign, it…
  • FAQ

    What are the Nyquist rates of GMSL2 and GMSL3 Links?

    The Nyquist rate is half the baud rate of a given signal. The baud rate is different from bit rate that it is the "number of changes in a signal per second" while bit rate is "number of bits per second…
  • FAQ

    What are the sources of insertion loss on the GMSL channel?

    ohmic losses along the PCB traces and cable conductors; dissipated power through the PCB and cable dielectric; and the resistance of the metal-to-metal interfaces of the connectors, In addition, impedance…
  • FAQ

    What are three ways to mitigate crosstalk interference in the PCB channel?

    Increase the distance between traces Add shielding Reduce the power of the crosstalk noise source
>