FAQ What is the eye mask for a GMSL system?

It is not applicable to have an eye mask for a GMSL system. Eye masks are only used on inputs which do not have equalization.  This is because many equalizers (GMSL included) can handle a completely closed eye.

To determine GMSL link compliance, meet the GMSL channel specification. 

To look at link performance, run a Link Margin test or the Link Inspection Tool, if available.