Yes, video interface to GMSL link repeater mode is supported by a limited number of devices that include those that may use common consumer connectors which often support HDCP data transmission. In the case of the GMSL family, this includes HDMI serializer and a limited number of DisplayPort serializers.
In addition, other GMSL devices may be used in repeater mode if a downstream HDCP link is connected and the application is determined to need HDCP repeater operation,