What are the main differences between DSI and CSI-2?
DSI is Display Serial Interface and is focused on display applications; CSI-2 is Camera Serial Interface and is focused on camera applications
GMSL2 DSI serializers accept only 24-bit RGB888 color
The physical layer (PHY) is the same for most cases, but packet processing will not work for mismatched MIPI interfaces