FAQ Can a single hardware design support both GMSL1 and GMSL2 operation?

A single design can meet requirements for both GMSL1 and GMSL2 operation if some very simple rules are followed: The system must meet the GMSL1 or GMSL2 channel specification. The GMSL link AC-coupling capacitors must be no smaller than 100nF/220nF if GMSL1 high immunity mode is/is not used. If PoC is used, the PoC network must be designed to work with all GMSL operating modes that may be used in the system.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.