Post Go back to editing

Output Power Usage of ADuM3070

Hello,

As mentioned in the datasheet of ADuM3070, we can get up to 2.5W output power with 5V input voltage. I  wonder up to what percentage of this output power can be occupied by the transformer. I mean, I'm plannig to use schematic in Figure 32 given in the datasheet and  a transformer having power rating lets say, 2.3W (instead of 2W) for Viso(+24V). On the other hand we have Vdd2(+5V) as an output voltage of ADuM3070. Is that possible? Its not briefly mentioned in the datasheet.

Thank you in advance!

Parents Reply Children
No Data