Post Go back to editing

ADuM3154 application that requires isolating two SPI slaves

Thread Summary

The user asks about the recommended approach for using two slaves with the ADuM3154 and the behavior of the MI pin when the chip is not selected. The final answer explains that the MSS signal is steered to the selected SS0/1/2/3 pin via the SSA0 and SSA1 selects, and these pins go to HiZ when not selected, requiring pull-up or pull-down resistors. The MI pin is driven regardless of the MSS signal state, so to avoid contention, the chip must be powered down when another device is communicating on the line.
AI Generated Content

1) What is the recommended approach when using only two slaves? We have two /SS pins available from the host MCU. It looks like we should connect the first slave select to /MSS, the second to SSA0, and fix SSA1.  

 

2) DS table 18, suggests that MI is driven even when the chip is not selected; if we want to have another device communicating on the line, we need to power down this chip to avoid contention on this line. Can you confirm this is the case? 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.