Post Go back to editing

Problem with ouput voltage VISO of ADUM6403

Hello,

we are using the ADUM6403 using 3.3V for the primary supply voltage and connect the Vsel pin to GNDiso. In this configuration the output voltage on the VISO pin can up to 5.04V instead of 3.3V.

The power supply voltage is good. We did also the following configuration:

- Vdd1 to 3.3V

- GND1 to GND

- Via, Vib, Vic, Vid are not connected

- Vddl to 3.3V (same used for Vdd1)

- GNDiso to GNDiso

- Vsel to GNDiso

- Vod, Voc, Vob, Voa are not connected

A resistor of 160Ohm is connected between the VISO pin and GNDiso. We have also connected a 0.1uF and a 10uF on the output VISO pin. On the tested device, the output voltage is 3.7V (see the attached file).

Do you have any ideas?

Thank you for your answers.

Sorry for my english

Parents
  • Brian:

    We check the voltages on the VIA, VIB, VID and VISO signals on another ADuM6403 which has the same behaviour. The volatges are the following:

    VIA = VIB = VID = 0V

    VISO = 4.1V

    Here the screen shoot:

    We also checked at power-up:

    None of the input signals are above 3.3V.

    We tried too with VIA, VIB, VIC, VID, VOA, VOB, VOC and VOD  left floating. The voltage on the VISO pin still 4.1V.

    Best Regards,

    Sebastien

Reply
  • Brian:

    We check the voltages on the VIA, VIB, VID and VISO signals on another ADuM6403 which has the same behaviour. The volatges are the following:

    VIA = VIB = VID = 0V

    VISO = 4.1V

    Here the screen shoot:

    We also checked at power-up:

    None of the input signals are above 3.3V.

    We tried too with VIA, VIB, VIC, VID, VOA, VOB, VOC and VOD  left floating. The voltage on the VISO pin still 4.1V.

    Best Regards,

    Sebastien

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.