Post Go back to editing

About ADuM6201 Output Voltage

Hi,

My customers are considering using ADuM 6201.
So I got a question.


It seems that we want to connect ADuM 142 and another ADuM 6201 behind Viso of ADuM 6201.

Since the regulator is contained in ADuM6201, I think that there is no problem.
Just to be sure, I'd like to confirm, but is there any problem connecting the two ICs to the power supply on the secondary side?

Best Regards,

Yuya

Parents
  • Hi, Brian

    Thank you for your reply.

    1, Thank you. understood.

    2, If you can not balance well with the two ICs, is that there is a possibility that it will not work as a   

     system?

    3, 3.3 V is required from VISO, and the current seems to need about 400 mA.

     I have not understood the ADuM 6201, but can we cover 400 mA in the first place?

     In the case of 3.3 V output, since it was described as 330 mW Output Power, I feel that it can only

     flow about 100 mA per piece.

    Best Regards,

    Yuya

Reply
  • Hi, Brian

    Thank you for your reply.

    1, Thank you. understood.

    2, If you can not balance well with the two ICs, is that there is a possibility that it will not work as a   

     system?

    3, 3.3 V is required from VISO, and the current seems to need about 400 mA.

     I have not understood the ADuM 6201, but can we cover 400 mA in the first place?

     In the case of 3.3 V output, since it was described as 330 mW Output Power, I feel that it can only

     flow about 100 mA per piece.

    Best Regards,

    Yuya

Children
No Data