Post Go back to editing

ADuM3470 Maximum Output Supply Current

Hi,

About How much current can the ADuM3470 supply with 3V input and 5V output ,4Mbps data rate?  

Can I use such a configuration? I guess that it can supply only less than about 165mA,  250mA x 3V/5V.
250mA is Iiso(MAX) specification with 3V input and 3V output,2Mbps.data rate. 

Parents
  • James:

    I think 165mA would be approximately the max output current to expect for 3.3V to 5V conversion.  I say approximately because if you use equation (1) on page 26 of datasheet you find that the turns ratio required would be greater than 2 (2.3), so the transformer needed for 3.3V to 5V would be the 1:3 turns ratio, part no JA4650-BL, but in this case using the circuit in figure 38.

    Regards, Brian 

Reply
  • James:

    I think 165mA would be approximately the max output current to expect for 3.3V to 5V conversion.  I say approximately because if you use equation (1) on page 26 of datasheet you find that the turns ratio required would be greater than 2 (2.3), so the transformer needed for 3.3V to 5V would be the 1:3 turns ratio, part no JA4650-BL, but in this case using the circuit in figure 38.

    Regards, Brian 

Children
No Data