Post Go back to editing

ADuM3470 Maximum Output Supply Current

Hi,

About How much current can the ADuM3470 supply with 3V input and 5V output ,4Mbps data rate?  

Can I use such a configuration? I guess that it can supply only less than about 165mA,  250mA x 3V/5V.
250mA is Iiso(MAX) specification with 3V input and 3V output,2Mbps.data rate. 

  • James:

    I think 165mA would be approximately the max output current to expect for 3.3V to 5V conversion.  I say approximately because if you use equation (1) on page 26 of datasheet you find that the turns ratio required would be greater than 2 (2.3), so the transformer needed for 3.3V to 5V would be the 1:3 turns ratio, part no JA4650-BL, but in this case using the circuit in figure 38.

    Regards, Brian 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.