Hi !
I have some questions about ADuM14x.
At our customers system sometime the device which is connected to ADuM14x input outputs HiZ.
So my question are these.
********************************************************************************************************************
Q1)
I already know that ADuM14x don't have internal resistor.
(ADuM14x)Does ADuM14x has internal Pull-up or Pull-down resistor?
What will happen if all supply are powered and input is HiZ.
I think output will be Indeterminate.
Is this correct?
Q2)
If our customer input HiZ to ADuM14x , would it cause some problem to the device?
For example, some kind of digital device will broke up when input is HiZ.
Q3)
At datasheet , this is written.
What do you mean
"The ADuM140D/ADuM140E/ADuM141D/ADuM141E/
ADuM142D/ADuM142E digital isolators require no external
interface circuitry for the logic interfaces."?
If there is HiZ input mode at system and if the customer want to control the output , I think they should insert Pull-up or down resistor to input pin.
Can our customer do this?
But at the datasheet "digital isolators require no external interface circuitry for the logic interfaces" so I want to ask can our customer insert resistor to the input signal line.
********************************************************************************************************************
Also the competitor chip has internal resistor so it won't be a problem if input is HiZ.
So if our customer have Pull-down/up resistor , it would become disadvantage.
Best regards.
Kawa