Hi
Is isolation type of ADuM5401 flyback?
I want to add current amount, I plan to connect multiple Vout.
Hi
Is isolation type of ADuM5401 flyback?
I want to add current amount, I plan to connect multiple Vout.
Hi:
For the ADuM5401 isoPower we use a tank circuit with the primary circuit coils the L, the parasitic capacitance the C and the switch resistance the R.
The ADuM5401 can be used with the output in parallel with the output of another isoPower device such as the ADuM5000, to obtain higher output current than one isoPower device. This is explained in figure 27 of the ADuM540x datasheet.
Regards, Brian