Post Go back to editing

ADUM4135 false FAULT signals latches device off

ADuM4135 going into error unexpectedly | EngineerZone 

  • We are using 4 off ADUM4135 in a power converter full bridge circuit, and are  seeing occasional FAULT signals, even though the DESAT pin is tied to GND2.

    We have VDD2 at 20V and VSS2 at -4V to drive SIC MOSFETs.

    Adding more decoupling right at the VDD2 pins didn't help, so we suspect some sort of radiated noise issue.

     

    To minimize some of the effects, we are considering linking the /FAULT and /RESET pins - any comments/ issues with that?

     

    Any support much appreciated.

    Thanks

     

    DM

Parents
  • Hello DM,

    Connecting nFault and nReset together is a valid configuration. When a fault is reported, the reset line will be automatically toggled. There is a time where the output of the ADuM4135 will be forced low, which is when the nReset is low. A pull-up resistor is needed in this configuration.

    I'll follow up with you directly.

    RSchnell

Reply
  • Hello DM,

    Connecting nFault and nReset together is a valid configuration. When a fault is reported, the reset line will be automatically toggled. There is a time where the output of the ADuM4135 will be forced low, which is when the nReset is low. A pull-up resistor is needed in this configuration.

    I'll follow up with you directly.

    RSchnell

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.