Post Go back to editing

Question about RS-485 Tranceiver

Hi All,

I'm looking for a RS-485 tranceiver chip covering the attached conditions.

- Maximam 64 tranceivers on the bus.

- Two types power supplies, 5V and 3.3V. 

Regards,

Kazu

QuestionaboutRS-485products.pdf
Parents
  • tnelson654 san,

    Thank you for supporting this case. The number of transceivers is maximum 64 pcs on the bus.

    ADM3085E is a little expensive to me, so I have a question about ADM3065E to you.

    Using ADM3065E under the following conditions are acceptable?

    1): Vcc=3.3V, Logic voltage=5V,   2): Vcc=5V, Logic voltage=3.3V

    **Logic voltage is not decided yet but it will be 3.3V or 5V.

    **Data rate needs 10M~20Mbps

    Regards,

    Kazu

Reply
  • tnelson654 san,

    Thank you for supporting this case. The number of transceivers is maximum 64 pcs on the bus.

    ADM3085E is a little expensive to me, so I have a question about ADM3065E to you.

    Using ADM3065E under the following conditions are acceptable?

    1): Vcc=3.3V, Logic voltage=5V,   2): Vcc=5V, Logic voltage=3.3V

    **Logic voltage is not decided yet but it will be 3.3V or 5V.

    **Data rate needs 10M~20Mbps

    Regards,

    Kazu

Children
No Data