Hello,
Please share me the Vil min and maximum input voltage requirement for A0,A1 and EN of ADG409
Regards,
Prasanna G
ADG409
Production
The ADG409 is a monolithic CMOS analog multiplexer comprising four differential channels. The ADG409 switches one of four differential inputs to a common...
Datasheet
ADG409 on Analog.com
Hello,
Please share me the Vil min and maximum input voltage requirement for A0,A1 and EN of ADG409
Regards,
Prasanna G
Hi Prasanna,
The max logic low voltage is 0.8V. The min logic low voltage is 0V/GND.
Regards,
Eric.
Hi Prasanna,
Vinh is the same as Vih, we typically use "in" instead of "i" on our datasheets. Our min logic high is 2.4V with max being Vdd. So you can drive with 3.3V.
Regards,
Eric.
Dear Eric,
Thank you for the quick response
I actually needed Vih min and Vih max for A0,A1 and EN of ADG409,
Our FPGA IO voh is 3.3 so Can i directly interface to ADG409, This is asking because in datasheet they mentioned "Input High Voltage of digital signal is VINH =2.4,Usually i can find vih but here Vinh what is the difference.
Regards,
Prasanna G