Dear Sir/Madam,
We will take the ADUM4160 for a project. For this project we need a double ore reinforced insulation from 1000 V/DC with the standard IEC61010. Is this possible with the ADUM4160? Are there any certifications about this?
ADuM4160
Production
The ADuM4160 is a USB port isolator, based on Analog Devices, Inc., iCoupler® technology. Combining high speed CMOS and monolithic air core transformer...
Datasheet
ADuM4160 on Analog.com
Dear Sir/Madam,
We will take the ADUM4160 for a project. For this project we need a double ore reinforced insulation from 1000 V/DC with the standard IEC61010. Is this possible with the ADUM4160? Are there any certifications about this?
Hello Compactelectric,
Unfortunately there is an issue with IEC61010 ed3 and our legacy designs that prevents us from getting that certification directly. These products predate edition 3 and one of the requirements of that standard is a 0.4mm loop height on the bond wires going across the isolated paddle. Without the correct loop height they will not issue a certification, and we can not go back and simply change the bonding height, it would invalidate multiple other certifications.
We are addressing this for new products that require IEC61010.
Many of our customers use VDE-0884-10 as a valid IEC equivalent standard to certify these products to reinforced for IEC61010 systems. The parts meet the IEC61010 standard in every other way.
Best Regards,
MSCantrell