To Whom it May Concern,
In regards to the ADuM7442S Digital Isolator. Is there a guaranteed state at the outputs at Power On?
The scenario is that the Input Side is powered, and the Output Side just becomes powered (the Power On Event), are the Outputs of the device guaranteed to go from the tri-state "Z" State to the Input's State without ever taking on the opposite state of the Input's State? I.E. A Power On glitch to the opposite state.
I hope that is clear .
Regards