Post Go back to editing

isolater Maximum Continuous Working Voltage

Hi

I have a question , Maximum Continuous Working Voltage.

This is ADM2484E DS.

It's written DC Voltage Basic Insulation 1066Vpeak , Reinforced Insulation 529Vpeak.

ADE7913 DS is , DC Voltage Basic Insulation 1173Vpeak . not have Reinforced Insulation.

And ADUM2211 is , DC Voltage 1130Vpeak.not have Reinforced Insulation.

How many is ADE7913 and ADUM2211  DC Voltage Reinforced Insulation ?

It has DC Voltage Reinforced Insulation which is about ADM2484E's Reinforced Insulation 529Vpeak ?

Best regards

HOD

Parents
  • Hi HOD,

    For the ADM2484E see Table 4:

    This part is certified to VDE 0884-10 with 849V peak reinforced working voltage.

    The part also has a 5000 V rms rating per UL1577.

    For the ADE7912/7913 see Table 2:

    These parts are certified to VDE 0884-10 with 846V peak reinforced working voltage.

    The part also has a 5000 V rms rating per UL1577.

    Best Regards,

    Richard

Reply
  • Hi HOD,

    For the ADM2484E see Table 4:

    This part is certified to VDE 0884-10 with 849V peak reinforced working voltage.

    The part also has a 5000 V rms rating per UL1577.

    For the ADE7912/7913 see Table 2:

    These parts are certified to VDE 0884-10 with 846V peak reinforced working voltage.

    The part also has a 5000 V rms rating per UL1577.

    Best Regards,

    Richard

Children
No Data