Post Go back to editing

isolater Maximum Continuous Working Voltage

Hi

I have a question , Maximum Continuous Working Voltage.

This is ADM2484E DS.

It's written DC Voltage Basic Insulation 1066Vpeak , Reinforced Insulation 529Vpeak.

ADE7913 DS is , DC Voltage Basic Insulation 1173Vpeak . not have Reinforced Insulation.

And ADUM2211 is , DC Voltage 1130Vpeak.not have Reinforced Insulation.

How many is ADE7913 and ADUM2211  DC Voltage Reinforced Insulation ?

It has DC Voltage Reinforced Insulation which is about ADM2484E's Reinforced Insulation 529Vpeak ?

Best regards

HOD

Parents
  • Hi HOD,

    We can help you to pick the best selection of parts to fit the customer's application. Please provide more details:

    • What is the customer's application? Energy metering?
      • On the front end there is an energy metering IC (ADE7913), and then on the back end there is a RS-485 comms (ADM2484E)?
    • Does the customer require basic or reinforced insulation?
    • What voltage levels are present in the customer's application? AC or DC, or both? And what levels?

    Best Regards,

    Richard

Reply
  • Hi HOD,

    We can help you to pick the best selection of parts to fit the customer's application. Please provide more details:

    • What is the customer's application? Energy metering?
      • On the front end there is an energy metering IC (ADE7913), and then on the back end there is a RS-485 comms (ADM2484E)?
    • Does the customer require basic or reinforced insulation?
    • What voltage levels are present in the customer's application? AC or DC, or both? And what levels?

    Best Regards,

    Richard

Children
No Data