ADUM5240
Production
The ADuM524x are dual-channel digital isolators with isoPower integrated, isolated power. Based on the Analog Devices, Inc. iCoupler® technology, a chip...
Datasheet
ADUM5240 on Analog.com
ADUM5200
Production
The ADuM520x are dual channel digital isolators with isoPower, an integrated, isolated dc-to-dc converter. Based on
the Analog Devices, Inc., iCouplerÂ...
Datasheet
ADUM5200 on Analog.com
Hi
I have a question ADUM5240.
Do you have a IBIS models for ADUM5240.
(I can see that ADUM5200 IBIS models .)
If you have another simulation models ( S parameters ,SPICE models ),Could you sent?
Best regards
HOD
HOD:
I have asked your question to the design engineer responsible for the ADuM5240, but there will be a delay in response because he is in China and they have a National holiday until next week. The ADuM5240 is older part, and we may not have an IBIS model, so I have also asked if the ADuM5200 IBIS model will do.
Regards, Brian
HOD: I asked the designer and he said that we don't have an IBIS model specifically for the ADuM5240, but that you can use the IBIS model for the ADuM5200 as it uses equivalent circuits.
Regards, Brian
Hi Brian
Thank you for your answer !
ADUM5200 will be considered as substitution.
When a IBIS model was taken in, VIA, VIB, VOA and VOB could normally take it in.
But VDD1, VISO, GND1 and GNDISO couldn't be taken in by an error.
If you know , please help .
Best Regards
HOD
HOD:
What is the detailed information for the error?
Regards, Brian
HOD:
I have asked the designer to look at the error and then I will respond.
Regards, Brian
HOD: I asked the designer to look at your issue with using the ADuM5200 IBIS for the ADuM5420 and here is the response:
I go through the ibis model files. Most probably, this issue is caused by wrong port mapping, ADuM1200 is more similar with ADuM5240.
The port mapping information for ADuM5200 is attached.
The port mapping information for ADuM1200 is attached.
The customer could try the model of ADuM1200. If it doesn’t work, please let the customer to modify the port mapping information in ADuM5200.ibs, changes as below:
1 VDD power
2 VIA input1
3 VIB input2
4 GND GND
5 GNDiso GND
6 VOB driver
7 VOA driver
8 Viso power
Regards, Brian