Post Go back to editing

ADuM144X creepage distance

We have a problem with one of your isolators ADuM1447 where from the datasheets package drawing the cheepage distance for the part is 5.6mm (enaugh for our purpose) but in the VDE report its stated 5.3mm (does not comply to standard in our case). Where is the error in your datasheet or in VDE report?

Parents
  • Hello;

    I always defer to the agencies measurements.  5.6mm on the drawing is the maximum body width under the JEDEC package standard. The drawing also says it could be as small as 5.0mm. 

    Unfortumately due to the way that JEDEC spedcifies their packages.  The creepage can not be reliabley determined from the drawing.  JEDEC tends to dump all of the packge tollerances onto the path that is required for creepage.  For example, there is no spec for the distance from the end pin to the end of the package .  In addition, there is a floating metal tie bar, that is required as part of the package manufacturing process, that must be subtracted from the creepage since it is right in the path.  Not problems for most products, but in isolation, it directly impacts the creepage.  So the agencies actually measure the package.  CSA measures 5.1mm, VDE measures 5.3.  Table 13 in the data sheet calls out 5.1 so we cover the worst case.

    For your issue, have you taken into account that our Mold compound is material group II.  That usually reduces the required creepage by about 33%.

    Best Regards,

    MSCantrell

Reply
  • Hello;

    I always defer to the agencies measurements.  5.6mm on the drawing is the maximum body width under the JEDEC package standard. The drawing also says it could be as small as 5.0mm. 

    Unfortumately due to the way that JEDEC spedcifies their packages.  The creepage can not be reliabley determined from the drawing.  JEDEC tends to dump all of the packge tollerances onto the path that is required for creepage.  For example, there is no spec for the distance from the end pin to the end of the package .  In addition, there is a floating metal tie bar, that is required as part of the package manufacturing process, that must be subtracted from the creepage since it is right in the path.  Not problems for most products, but in isolation, it directly impacts the creepage.  So the agencies actually measure the package.  CSA measures 5.1mm, VDE measures 5.3.  Table 13 in the data sheet calls out 5.1 so we cover the worst case.

    For your issue, have you taken into account that our Mold compound is material group II.  That usually reduces the required creepage by about 33%.

    Best Regards,

    MSCantrell

Children
No Data