the rating of the sink current of ADM3051 RXD pin

Device : ADM3051.

Please teach me the rating of RXD the sink current.

I would like to drive the photocoupler using the H/L of RXD.
Insert the resistance, drive current of the photo-coupler is 10mA.
So RXD pin,Current is 10mA sink.

I attach a rough image.

The data sheet P3 there is the following description.
Output Voltage Low(0-1.5V) : IOUT = 10 mA
Is it the rating of the sink current?

Thank you.

ADM3051.pptx
Parents
  • 0
    •  Analog Employees 
    on Feb 23, 2016 9:34 AM

    Hi Yoshinari-san,

    When the ADM3051 CAN device is receiving data from the bus:

    for a logic 0 / low (CAN bus dominant state) at the RO there is up to 10 mA available.

    For the CAN bus recessive state:

    there is up to 100uA available at the RO.

    Regards,

    Richard

Reply
  • 0
    •  Analog Employees 
    on Feb 23, 2016 9:34 AM

    Hi Yoshinari-san,

    When the ADM3051 CAN device is receiving data from the bus:

    for a logic 0 / low (CAN bus dominant state) at the RO there is up to 10 mA available.

    For the CAN bus recessive state:

    there is up to 100uA available at the RO.

    Regards,

    Richard

Children
No Data