Hi All, I want to try the ADP5586 but it's a bga. Is there a thru hole version available so when code is written for it I don't have to start all over again?
Thanks,
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADP5586
Production
The ADP5586 is a 10-input/output port expander with a built-in keypad matrix decoder, programmable logic, reset generator, and pulse generators. Input...
Datasheet
ADP5586 on Analog.com
Hi All, I want to try the ADP5586 but it's a bga. Is there a thru hole version available so when code is written for it I don't have to start all over again?
Thanks,
Hello bcavan,
Unfortunately, the ADP5586 only comes in a WLCSP (BGA) package. It was designed with tight spaces in mind. The sister chip to the ADP5586 is the ADP5585. They program up very similarly, and the ADP5585 can come in the LFCSP package which is easier to solder. Please check out if the ADP5585 can meet your needs.
We also have evaluation boards available to aid in prototyping.
RSchnell