ADM3053 VISOOUT

We would like to supply power to the CAN and the other circuit by using the output from the VISOOUT.
Other circuit is a logic circuit, it is scheduled to about 20mA current.

Do you support such usage ADM3053?

 

Thank you.

  • 0
    •  Analog Employees 
    on Dec 21, 2015 2:31 PM

    Hi Yoshinari-san,

    The ADM3053 DC-DC VISO is designed to support the CAN transceiver integrated in the ADM3053 package.

    Due to the CAN transceiver VISO current requirements, very little current is available to support external devices.

    The VISO would not be able to reliably support providing 20 mA externally to power another device.

    Regards,

    Richard