Post Go back to editing

ADuM1401 input

We’ve been doing some tests on above, and get considerable oscillation on output when i/p risetime is 100us or so. Please see attached screenshot: yellow trace is i/p signal, 4.9v p-p, risetime of 100us (ignore Y axis scale for signal – x10 probe attached). Blue trace is o/p signal – as you can see, any amount of noise on i/p is giving rise to multiple o/p transients.

Is there any form of hysteresis on the input? The datasheet implies it’s Schmitt but it doesn’t act like it. Is there a pin for pin compatible device which does have Schmitt inputs?

Parents
  • Hi Jian,

    We don’t know how much noise. The signal is low freq TTL signal sent over long line so we have CR filter at input to reduce any noise picked up.

    We assumed standard TTL schmidt type hysteresis 300mV min (ADuM1401 data sheet does not spec it).

    However have found replacement Silicon Labs device Si8640 series with min 380mV hysteresis which works fine!

      Tony Haywood

Reply
  • Hi Jian,

    We don’t know how much noise. The signal is low freq TTL signal sent over long line so we have CR filter at input to reduce any noise picked up.

    We assumed standard TTL schmidt type hysteresis 300mV min (ADuM1401 data sheet does not spec it).

    However have found replacement Silicon Labs device Si8640 series with min 380mV hysteresis which works fine!

      Tony Haywood

Children
No Data