ADUM1410 and ADUM1412 problem

Hi,

 
We are having a big problem of reliability components  ADUM
1410 ADUM1412 we use in a system under railway.
Here are the typical electrical interface we use components.
 
As you can see from the diagram the nominal 24VDC supply is removed from  the
vehicle with the power inputs properly protected.
The problem is evident only when we install our equipment on the vehicle in  a
particularly disturbed. 
In the laboratory it has never shown any problem, also the device has  passed
all the necessary tests to EN 50155 certification.
The problem we are encountering is the following. 
Randomly and without a logical explanation some components undergo  alterations
of their characteristics, but there were no malfunctions, 
if the operating temperature is below the 40/45 ° C. 
As this temperature is exceeded the component stops working because the  input
of the 5V power supply is short-circuited.
In this condition, the power supply enters the protection and de- energises
the component. 
After about 1 second the feeder attempts to return power to the component  but,
this remaining in short circuit back into the power supply protection.  
This behavior, with a duty cycle of 1 sec. continues until the temperature
drops below the threshold of 40/45 ° C.
 
Can you give us an explanation for this strange behavior of ADUM Thank you  

Best regards
 
M. Menichini

  • It's possible that a transient on the +5Va supply is inducing latch-up. Can you see any disturbances on this line at the ADuM141x VDD pins? The 100 nF decoupling caps should be on the same side of the board as the IC and as close to the VDD pin as possible. If you are seeing transients, ensure that they are within the Absolute Maximum Ratings of the device. If so, you can try adding a 200 ohm resistor in series with the VDD pin (before the decoupling cap) to see if that improves the situation.

    DaveC

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin