Hi,
I don't see any ESD specifications for AMD4850ARMZ. Is there any ESD protection available for this IC or do i need to use an external ESD protection diodes to use this?
Regards,
Akhil
Hi,
I don't see any ESD specifications for AMD4850ARMZ. Is there any ESD protection available for this IC or do i need to use an external ESD protection diodes to use this?
Regards,
Akhil
Hi Akhil,
The ADM4850 has a basic level of HBM ESD protection at 2 kV.
The ADM4850 also has a basic level of CDM ESD protection at 1.5 kV.
What is your application? Is your application in a harsh EMC environment?
Regards,
Richard
Hi Akhil,
Just an extra note -- ADI also has a range of more ESD robust RS-485 transceivers at 3V and 5V operation:
5 V operation:
ADM485E, ADM487E, ADM1487E have 15 kV HBM ESD protection
3 V operation:
ADM3070E - ADM3078E have 15 kV HBM ESD protection
Best Regards,
Richard
Hi Akhil,
Thanks for the feedback on the product application.
Regards,
Richard
The application is a Medical laboratory Equipment.
Thanks,
Akhil