Post Go back to editing

2KV High-side, low-current measurement

Is it possible to use an AD620 connected to an AD210 to measure high-side current through a sampling resistor?  With the REF line on the AD620 and the Icom line on the AD210 connected to the bottom of the resistor (and the top of the resistor is connected to 2KV).  The REF/Icom voltage measured with respect to ground would be very close to 2KV. 

If I were to do that what ground referenced voltage would I measure at +VISS on the AD210?  Would it be 2KV - Rsense*Iload + 15V?  That is, assuming I didn't let the smoke out.  ;-)

Are there any common mode limits I need to be careful to watch out for?

Parents
  • Thanks DaveC, I pulled the datasheet and the AD7403 is a very nice part.  Since I need to get to digital values eventually I was excited to see that too.  Unfortunately, I don't know how to power the input side.

    The designs I have seen typically use a zener to produce voltages of the right separation.  That is, VDD1 would connect to the 2KV power supply output and GND1 would connect to the anode side of a 5.1V zener.  This floats the whole input side up into the 2KV range.  Similarly, VIN+ would connect to the 2KV power supply output and VIN- would connect to the bottom of the sense resistor.  Nothing wrong with that as far as I can tell... at least with respect to the voltage levels.  Is that how it would typically be connected?

    BUT, here is my problem.  The high-voltage supply I would like to use is only 2.4 mW.  I don't think I have enough output power to drive the Zener into breakdown and power the AD7403.

    The AD210 is attractive because I don't think I need to rely on the high-voltage supply to provide the power for the device itself.  The part derives the isolated power for the HV side with it's 3-port configuration.  I'm not entirely confident about the connections on the HV side.  Of course when confronted with an $80 part, it might be easier, cheaper, to use a HV supply with a little more oomph.

    I haven't used any of these parts before so I don't know their capabilities and limitations... particularly related to the high-voltage side. 

Reply
  • Thanks DaveC, I pulled the datasheet and the AD7403 is a very nice part.  Since I need to get to digital values eventually I was excited to see that too.  Unfortunately, I don't know how to power the input side.

    The designs I have seen typically use a zener to produce voltages of the right separation.  That is, VDD1 would connect to the 2KV power supply output and GND1 would connect to the anode side of a 5.1V zener.  This floats the whole input side up into the 2KV range.  Similarly, VIN+ would connect to the 2KV power supply output and VIN- would connect to the bottom of the sense resistor.  Nothing wrong with that as far as I can tell... at least with respect to the voltage levels.  Is that how it would typically be connected?

    BUT, here is my problem.  The high-voltage supply I would like to use is only 2.4 mW.  I don't think I have enough output power to drive the Zener into breakdown and power the AD7403.

    The AD210 is attractive because I don't think I need to rely on the high-voltage supply to provide the power for the device itself.  The part derives the isolated power for the HV side with it's 3-port configuration.  I'm not entirely confident about the connections on the HV side.  Of course when confronted with an $80 part, it might be easier, cheaper, to use a HV supply with a little more oomph.

    I haven't used any of these parts before so I don't know their capabilities and limitations... particularly related to the high-voltage side. 

Children
No Data