Post Go back to editing

ADUM2251 Side2 Slave don't respond

Hello,

I have a design (see Appendix), that makes some communication problems.

I have double-checked logic low level thershold and it is more than 0,9V since

Vcc and Vcc-p is 5V.

I have read this thread

https://ez.analog.com/message/75240#75240

and  I have also watched the Video from MSCantrell "How I2C Isolators work"

Video which is super helpfull.

When I use the digital Isolator for some reasons the MAX1238, don't pull down the data-line when

it should transmit the data-pattern. With no digital isolator everything works fine.

Has anybody an idea or hint ?

Thanks for your support.