Comparable device to ADUM6000 but with higher efficiency

Is there a comparable device to the ADUM6000, but with higher efficiency? The ADUM6000 has up to 31% efficiency.

Parents
  • 0
    •  Analog Employees 
    on Oct 10, 2014 6:21 AM

    John:

    There is not another device that I know of that meets the features that the ADuM6000 has: small size, isolated dc to dc converter with 5000V rms isolation. The ADuM4070 has a higher efficiency of 70 -80% and meets the 5000Vrms isolation, but has a larger size solution. This solution requires an external transformer, diode and coil.The transformer vendors are Coilcraft and Halo, and for 5000V isolation the Halo is much smaller.

    Regards,  Brian

Reply
  • 0
    •  Analog Employees 
    on Oct 10, 2014 6:21 AM

    John:

    There is not another device that I know of that meets the features that the ADuM6000 has: small size, isolated dc to dc converter with 5000V rms isolation. The ADuM4070 has a higher efficiency of 70 -80% and meets the 5000Vrms isolation, but has a larger size solution. This solution requires an external transformer, diode and coil.The transformer vendors are Coilcraft and Halo, and for 5000V isolation the Halo is much smaller.

    Regards,  Brian

Children
No Data