Hi
I saw UG-304 Figure17 and 18.
ADuM1250 side1 is connected to ADM1075, I think.
Is it correct connection?
I think, a command trigger should be connected to side1.
Regards
moto
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
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
ADUM1250
Production
The ADuM1250 / ADuM1251 are hot swappable digital isolators with non-latching, bidirectional communication channels compatible with I2C interfaces. This...
Datasheet
ADUM1250 on Analog.com
ADM1075
Last Time Buy
The ADM1075 is a full feature, negative voltage, hot swap controller
with constant power foldback and high accuracy digital current
and voltage measurement...
Datasheet
ADM1075 on Analog.com
Hi
I saw UG-304 Figure17 and 18.
ADuM1250 side1 is connected to ADM1075, I think.
Is it correct connection?
I think, a command trigger should be connected to side1.
Regards
moto
Hello Moto,
Side 1 of the ADuM1250 uses non standard levels as part of its flow of control scheme. The ADM1075 also has non standard levels on its SCL and data lines. So in this configuration I would recommend using Side 2 facing the ADM1075, since side 2 has standard CMOS output levels, there will be no issue detecting a low output. Whether you can do this really depends on the details of what is connected to the isolated I2C bus and what its I/O levels are.
However, since you have a split data line, you have other options in the iCoupler line. For example you could use the ADuM144x ultra low power device. It will allow you to power from the 48V bus without squandering a lot of power. The data line is split on one side, and the Data in and out can be combined on the isolated side with a tri state buffer to allow I2C bidirectional capability as shown in the diagram below. This is for a POE controller, but the principle is the same. This type of arrangement will work with a wide variety of our standard digital isolators.
I hope this gives you some help and options.
Best regards,
MSCantrell
Hello Moto,
Side 1 of the ADuM1250 uses non standard levels as part of its flow of control scheme. The ADM1075 also has non standard levels on its SCL and data lines. So in this configuration I would recommend using Side 2 facing the ADM1075, since side 2 has standard CMOS output levels, there will be no issue detecting a low output. Whether you can do this really depends on the details of what is connected to the isolated I2C bus and what its I/O levels are.
However, since you have a split data line, you have other options in the iCoupler line. For example you could use the ADuM144x ultra low power device. It will allow you to power from the 48V bus without squandering a lot of power. The data line is split on one side, and the Data in and out can be combined on the isolated side with a tri state buffer to allow I2C bidirectional capability as shown in the diagram below. This is for a POE controller, but the principle is the same. This type of arrangement will work with a wide variety of our standard digital isolators.
I hope this gives you some help and options.
Best regards,
MSCantrell