Hi
I saw UG-304 Figure17 and 18.
ADuM1250 side1 is connected to ADM1075, I think.
Is it correct connection?
I think, a command trigger should be connected to side1.
Regards
moto
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
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
ADUM1250
Production
The ADuM1250 / ADuM1251 are hot swappable digital isolators with non-latching, bidirectional communication channels compatible with I2C interfaces. This...
Datasheet
ADUM1250 on Analog.com
ADM1075
Last Time Buy
The ADM1075 is a full feature, negative voltage, hot swap controller
with constant power foldback and high accuracy digital current
and voltage measurement...
Datasheet
ADM1075 on Analog.com
Hi
I saw UG-304 Figure17 and 18.
ADuM1250 side1 is connected to ADM1075, I think.
Is it correct connection?
I think, a command trigger should be connected to side1.
Regards
moto
ADM1075 input high level is 1.1V min and low level is 0.8V max.
it is a little different from normal I2C, so Side 1 connection might be no problem.
but please tell us which is better.
moto
ADM1075 input high level is 1.1V min and low level is 0.8V max.
it is a little different from normal I2C, so Side 1 connection might be no problem.
but please tell us which is better.
moto