any solution for lvds driver from FPGA

I use cyclone FPGA to get lvds signals. The project need drive lvds for a long distance . I find ADN4665 and ADN4666 ,but I can not find the clock driver . Can anybody give me some sugestions?

  • 0
    •  Analog Employees 
    on Jun 13, 2013 6:35 PM over 7 years ago

    Hello Niulian,

    If I understand correctly, you want to buffer the LVDS outputs from the FPGA in order to drive them across a longer distance?

    What distance do you want to drive across, and at what clock/data speeds? What is at the receiving end?

    The ADN4670 acts as a buffer suitable for LVDS clock signals up to 1.1GHz. This also provides 1:10 fan-out, but unused outputs can be disabled.

    Alternatively, an LVDS receiver such as ADN4666 (or ADN4662/ADN4664/ADN4668) can be connected to the FPGA outputs, and then an LVDS driver such as ADN4665 (or ADN4661/ADN4663/ADN4667) can be connected to the ADN4666 receiver outputs.

    Best regards,

    Conal

  • 0
    •  Analog Employees 
    on Aug 2, 2018 4:53 PM over 2 years ago
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin