Post Go back to editing

ADM238L pin-matching alternative

Hello,

We have been using the ADM238LJRZ in a "mature" product line with thousands of systems operating in the field. In some cases, the negative charge pump has been found to be damaged when cable lengths between devices are longer than approx 50 feet, which appears to have created conditions where wire capacitances exceed maximum allowable values. A detailed Failure Analysis confirmed that an EOS "event" had damaged the charge pump causing abnormally low output voltage. We are looking at implementing a TVS/Zener solution to mitigate this susceptibility but wonder if there might be a pin-to-pin alternative available that is inherently more robust than the ADM238L? As a side question, is there an established test method for this type of issue? One that could recreate the EOS damage and then be used to know that a TVS solution is working?

Best regards,

Mark

Parents
  • Hi Mark,

    The ADM208EARZ may be an option. This is a pin compatible device with ESD hardened RS-232 pins up to 15kV.

    I'm not that familiar with test methods for ESD type issues. The only way I can think over verifying this is to zap the RS-232 pins with an ESD gun to try to replicate the issue on the ADM238L. Then try the same test with the ESD hardened ADM208E device to verify the issue is resolved.

    I'd expect to see some data errors if the cable length and capacitance gets too large. Worth keeping an eye on this and using low capacitance cables if you have to use very long cables.

    Rgds,

    Paul

Reply
  • Hi Mark,

    The ADM208EARZ may be an option. This is a pin compatible device with ESD hardened RS-232 pins up to 15kV.

    I'm not that familiar with test methods for ESD type issues. The only way I can think over verifying this is to zap the RS-232 pins with an ESD gun to try to replicate the issue on the ADM238L. Then try the same test with the ESD hardened ADM208E device to verify the issue is resolved.

    I'd expect to see some data errors if the cable length and capacitance gets too large. Worth keeping an eye on this and using low capacitance cables if you have to use very long cables.

    Rgds,

    Paul

Children
No Data