Hi,
Please let me ask to confirm the description on datasheet of ADuM5402, in case 3.3V primary (VDD1) / 3.3V secondary (Viso)
such as below.
Here, recommended operation range for VDD1 is, 3.0 V ≤ VDD1 ≤ 3.6 V.
Question is, at Setpoint in 1st row, shows Viso is 3.0 V ≤ Viso ≤ 3.6 V. Does it mean,
a) Viso is determined by actual value of Vdd1 with in the above range ? In other words, if Vdd1 is 3.5V for example, Viso will be around 3.5V uniquely ?
or
b) Despite what voltage of VDD1 is, Viso will be in the range of 3.0 V ≤ Viso ≤ 3.6 V ? In other words, even if Vdd is quite stable around 3.5V, Viso can be 3.0 V ≤ Viso ≤ 3.6 V ?
Your confirmation would be very much appreciated.
Best Regards,