Hi,
can I use the ESD Protection as per schematic on the ADuM4160? [It is to be on a peripheral]
PS- I do NOT want to use the PiC's VUSB in this case...
Thanks again!
PS:The process to get to this result is shown below:
ADuM4160
Production
The ADuM4160 is a USB port isolator, based on Analog Devices, Inc., iCoupler® technology. Combining high speed CMOS and monolithic air core transformer...
Datasheet
ADuM4160 on Analog.com
Hi,
can I use the ESD Protection as per schematic on the ADuM4160? [It is to be on a peripheral]
PS- I do NOT want to use the PiC's VUSB in this case...
Thanks again!
PS:The process to get to this result is shown below:
Hello Yachaan,
I don't see any reason this implementation would be a problem.
MSCantrell
Hello Yachaan,
After seeing the entire thing, I have a couple of comments.
1) the protection is to stop ESD and EOS from the cable being applied to the chip. Please review whether the ESD protection…
Hello Yachaan
On the upstream side, the ADuM4160 has an integrated pullup, and you would be doubling up. So definitely do not use an integrated pull-up on the upstream side.
I don't see that you need…
Like so?
What I like about this - it replaces all separate components - like resistors.
They should be internally matched too.
So, depending if the peripheral has got its own pull-up or not,
you would connect [ or not ] the 3.3V built in zener on the downstream side
[and here it is needed].
Correct?
Hello Yachaan,
The more I look at these termination networks the less I like them. I do not think that they are the correct part to place with our coupler. Our part has its own termination resistors, 15K pull downs on the downsream side and 1.5k pull up on the upstream side. These networks also contain these components, so they can not be used. We have tried the ON Semiconductor NUP4202W1 type devices and found them to do the job. They provide ESD protection on the input lines and link to the Vbus for bias and ESD protection. You should not need one of these networks on the downsream side, just on the upstream side between the connector and the ADuM4160. Please consider changing to a single protection device similar to the NUP4202W1.
MSCantrell
That looks more like it.
MSCantrell