Hi,
can I use the ESD Protection as per schematic on the ADuM4160? [It is to be on a peripheral]
PS- I do NOT want to use the PiC's VUSB in this case...
Thanks again!
PS:The process to get to this result is shown below:
ADuM4160
Production
The ADuM4160 is a USB port isolator, based on Analog Devices, Inc., iCoupler® technology. Combining high speed CMOS and monolithic air core transformer...
Datasheet
ADuM4160 on Analog.com
Hi,
can I use the ESD Protection as per schematic on the ADuM4160? [It is to be on a peripheral]
PS- I do NOT want to use the PiC's VUSB in this case...
Thanks again!
PS:The process to get to this result is shown below:
Hello Yachaan,
I don't see any reason this implementation would be a problem.
MSCantrell
Hello Yachaan,
After seeing the entire thing, I have a couple of comments.
1) the protection is to stop ESD and EOS from the cable being applied to the chip. Please review whether the ESD protection…
Hello Yachaan
On the upstream side, the ADuM4160 has an integrated pullup, and you would be doubling up. So definitely do not use an integrated pull-up on the upstream side.
I don't see that you need…
Hello Yachaan,
Yes, I think this is the correct connection for the protection devices.
The ADuM3440 is probably not the best part for limit switch application. This part is our highest speed coupler, and we eliminated the glitch filter in favor of high throughput. A lower cost solution would be the ADuM3400A which is slower, and has a glitch filter. One is a drop in replacement for the other.
Good luck.
Hello Yachaan,
Yes, I think this is the correct connection for the protection devices.
The ADuM3440 is probably not the best part for limit switch application. This part is our highest speed coupler, and we eliminated the glitch filter in favor of high throughput. A lower cost solution would be the ADuM3400A which is slower, and has a glitch filter. One is a drop in replacement for the other.
Good luck.