Hi,
can I use the ESD Protection as per schematic on the ADuM4160? [It is to be on a peripheral]
PS- I do NOT want to use the PiC's VUSB in this case...
Thanks again!
PS:The process to get to this result is shown below:
ADuM4160
Production
The ADuM4160 is a USB port isolator, based on Analog Devices, Inc., iCoupler® technology. Combining high speed CMOS and monolithic air core transformer...
Datasheet
ADuM4160 on Analog.com
Hi,
can I use the ESD Protection as per schematic on the ADuM4160? [It is to be on a peripheral]
PS- I do NOT want to use the PiC's VUSB in this case...
Thanks again!
PS:The process to get to this result is shown below:
Hello Yachaan,
I don't see any reason this implementation would be a problem.
MSCantrell
Hello Yachaan,
After seeing the entire thing, I have a couple of comments.
1) the protection is to stop ESD and EOS from the cable being applied to the chip. Please review whether the ESD protection…
Hello Yachaan
On the upstream side, the ADuM4160 has an integrated pullup, and you would be doubling up. So definitely do not use an integrated pull-up on the upstream side.
I don't see that you need…
Hi, thanks for the interest.
1] I try to protect my PC from this board and the stepper drivers further down the line.
So it is the other way around.
I thought i was going to show you a correction. BUT:
An app note:
Should I not get rid of the pull-up resistor at the input side? [No VDD]
Alternatively, here is two resistors at the input - how would this affect the USB setup?
Hi, thanks for the interest.
1] I try to protect my PC from this board and the stepper drivers further down the line.
So it is the other way around.
I thought i was going to show you a correction. BUT:
An app note:
Should I not get rid of the pull-up resistor at the input side? [No VDD]
Alternatively, here is two resistors at the input - how would this affect the USB setup?