Hi,
can I use the ESD Protection as per schematic on the ADuM4160? [It is to be on a peripheral]
PS- I do NOT want to use the PiC's VUSB in this case...
Thanks again!
PS:The process to get to this result is shown below:
Hi,
can I use the ESD Protection as per schematic on the ADuM4160? [It is to be on a peripheral]
PS- I do NOT want to use the PiC's VUSB in this case...
Thanks again!
PS:The process to get to this result is shown below:
Hello Yachaan,
I don't see any reason this implementation would be a problem.
MSCantrell
Hello Yachaan,
After seeing the entire thing, I have a couple of comments.
1) the protection is to stop ESD and EOS from the cable being applied to the chip. Please review whether the ESD protection…
Hello Yachaan
On the upstream side, the ADuM4160 has an integrated pullup, and you would be doubling up. So definitely do not use an integrated pull-up on the upstream side.
I don't see that you need…
Hello Yachaan,
After seeing the entire thing, I have a couple of comments.
1) the protection is to stop ESD and EOS from the cable being applied to the chip. Please review whether the ESD protection should be referenced to the 5V line instead of the 3.3V line. The configuration shown would not protect the regulator.
2) the primary USB interface looks good, your PIC is a peripheral and the upstream side is powered from the cable.
I can't read the option section, what are you doing with the other isolation and connectors?
Good luck
Hello Yachaan,
After seeing the entire thing, I have a couple of comments.
1) the protection is to stop ESD and EOS from the cable being applied to the chip. Please review whether the ESD protection should be referenced to the 5V line instead of the 3.3V line. The configuration shown would not protect the regulator.
2) the primary USB interface looks good, your PIC is a peripheral and the upstream side is powered from the cable.
I can't read the option section, what are you doing with the other isolation and connectors?
Good luck