Post Go back to editing

ADUM2250 Working Voltage & Regulation Questions

I'm very new to insulation standards, so I have a few questions.

What I'm pretty sure on is our box will need double or reinforced insulation.  We will most likely be using I2C and probably will insulate the rest of the circuit from our high voltage inputs going into an ADE7878.  The plan is to use the ADUM2250 and some other unidirectional iCouplers for the HSDC (high-speed data capture lines) going between the ADE7878 and a microcontroller (and the rest of the circuit).  We'll need a DC-DC converter to get isolated power over to the ADE7878, of course.

Our box will measure up voltages up to 345 V line-to-neutral (600 V line-to-line) on the voltage inputs to the ADE7878.  Readings can be read over Ethernet too.  So it appears our box falls under the IEC 61010-1 standard for test-and-measurement equipment as well as IEC 60950-1 for information technology equipment.

I have a copy of 61010-1 that's about a year old, but from it it seems for basic insulation we need 3,320 VACrms and a clearance/creepage of 5.5 mm. 

# 1. One question I have, do these voltages and clearances differ between 61010-1 and 60950-1?

Looking over the ADUM2250 spec sheet, I see that it has a minimum 7.7mm creepage and 8.0mm clearance.  Since it provides isolation of 5kVACrms too, it appears to meet the needs for basic insulation regarding IEC 61010-1.

# 2. Am I interpreting that correctly?

This FAQ question says that all iCoupler meet at least 400 VACrms but I'm a bit confused because the table seems to imply even for the ADUM225x series that it only supports 400 VACrms working voltage for a bipolar AC waveform, contradicting the spec sheet.  That page doesn't specify which standard that is met either.

# 3. So in order to achieve double insulation, one solution is to put two ADUM2250's back-to-back with isolated supplies from DC-DC converters?

# 4. I'm a little unclear about section 6.5.3 of IEC 61010-1 regarding protective impedances.  Would a pair of resistors in series with the voltage input line count (such as in the voltage divider)?  So you would only need one ADUM2250 along with the resistors?

Parents
  • Hi Mark

      Thanks for that info, we had originally thought we could use 60950 for various parts of our design, however we were informed that the device will fall more into 61010..

    The area in the design where these devices would cross is between the safe control board, and a section of circuitry that is exposed directly to DC voltages of around 200V, eg recording output voltages and currents, driving thyristors etc.

    The 200V side is the output part of a Geophysical transmitter and its driving powersupply, potentially hazardous..

    We'll have a chat to our compliance guys.

    Just out of interest where in the standard exactly is it that these components no longer meet the requirements?

    Thanks

       Richard

Reply
  • Hi Mark

      Thanks for that info, we had originally thought we could use 60950 for various parts of our design, however we were informed that the device will fall more into 61010..

    The area in the design where these devices would cross is between the safe control board, and a section of circuitry that is exposed directly to DC voltages of around 200V, eg recording output voltages and currents, driving thyristors etc.

    The 200V side is the output part of a Geophysical transmitter and its driving powersupply, potentially hazardous..

    We'll have a chat to our compliance guys.

    Just out of interest where in the standard exactly is it that these components no longer meet the requirements?

    Thanks

       Richard

Children
No Data