Post Go back to editing

Using multiple RS232 isolation channels

Hi,

We were considering the use of ADM3251E for multiple channel RS232 isolation, in which we may use upto 9 chips (A future products may use 17 channels). But I find that use of 9 x ADM3251E would need more than 1A supply current which is not acceptable. I am also worried about the EMI issue if there are so many isolation chips on a single PCB. Can you suggest a way to achieve this by using lesser current? The overall cost of the solution should not exceed the cost of the ADM3251E based solution. I was considering ADM3252E which appears to be more efficient, but I found the cost to be on the higher side at $ 8.49 compared to $ 2.99 for ADM3251 even if I were to use the ADM3252 for 2 channels.  Please suggest a way out. Also please let me know the EMI related precautions that we may have to take in handling so many isolated channels.

Regards,

Hemant

  • I moved this question to the Interface and Isolation community.  Someone here should be able to assist you.

  • Hi Hemant,

    As you suggest the ADM3252E will be more efficient solution than the ADM3251E. It also has other advantages in that it is a more compact dual channel solution, can run off 3.3V without powering VISO side, etc.

    In your case with such a large number of channels the other solution would be to use separate RS232 and icoupler devices. There are a number of RS232 parts to choose from depending on your combination of Tx and Rx channels, Vcc voltage, ESD protection, etc. The ADM3315E x 3 may be a suitable option as it has 3 Tx and 3 Rx channels, runs off 3.3V supply and has 15kV ESD protection on RS232 I/O pins. There are other parts with more channels as well.

    In terms of iCouplers, the choice depends on the isolation rating required and whether you need isolated power or not. Assuming just isolated RS232 at 2.5kV then something like the ADuM1402 which has 2 isolation channels in each direction.

    Rgds,

    Paul

  • Hi Paul,

    Thank you for the response. Since our usage demands only low speed transmit/receive and ground for isolated RS232 port, I thought of using a combination of ADUM5201 for power and isolation, and ADM101E(or equivalent) for level conversion. This may be equivalent to ADM3251E, but will need much less current on the primary side, which should not exceed 25-30 mA even when RS232 is loaded. The cost of two chips could be higher than that of ADM3251E, but the benefit of saving close to 700mA current while using 9 channels will bring other benefits too. If I need more control signals, I will think of adding ADUM141X devices and low power RS232 level converters such as ADM3315E while deriving isolated power for them from the ADUM5201. What do you think?

    Do you also think a separate ESD surge suppressor diodes be used at the ADM101E's RS232 pins?

    Regards,

    Hemant

  • Hi Hemant,

    The ADM101E works off a 5V supply and has a lower Txout output voltage swing so doesn't require the additional voltage doubler capacitors that you need on other RS232 parts. If you have a suitable 5V supply from the ADuM5201 and the output levels are sufficient (which they probably are as you mention you only require low speed transmit/receive) then the ADM101E is probably a good fit. The ADM101E also has 15kV ESD protection on the I/O pins so I don't think any extra protection will be required. Just ensure that you use low ESR capacitors for Vcc and V- pins (e.g. X5R, X7R series).

    Rgds,

    Paul

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin