Adum3472

I have interest in use Adum3472 to isolate two micro controlers and DSS and VGA.

The problem is: in side A I have a Li-On cell (3V to 4.2V) and in side B I need +5V and -5V and based in DataSheet Adum34x function only in range of 3 to 3.6V or 4 to 5V. I need input range of 3 to 4.2V.

Is posible?

If obtain only +5 in the output is't OK.

Thank you in advance.

Aldo Ferszt

General Manager

Parents
  • 0
    •  Analog Employees 
    on Aug 2, 2018 4:33 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin
Reply
  • 0
    •  Analog Employees 
    on Aug 2, 2018 4:33 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin
Children
No Data