medical ADC isolation

Hi

I would like to read temperature from thermistor connected to catheter (medical device)

using the following thermistor P12358CT-ND, THERMISTOR NTC 10K OHM 5% 0201

MCU is arduino uno board

after reading I found the AD7400 and  AD7400A and have a few question

1) for what and how I use the internal clock? (or way both of them have MCLKI if one does have internal clock?)

2) are they good enough for medical 60601-1 ISO (5 kv resistance), can not find "60601" in their spec

I am not and HW person so I am looking for simple EVM just plug and run (a full solution)

3) is there a ADC fully integrated 5 kV rms  signal and power isolated like the adm2687E

4) I found the EVAL-AD7400/AD7401, how do I connect isolated dc to the digital side (simple dc-dc convertor?)

5) is there a description how to connect it to MCU including power isolation (or better a link for a EVAL doing it already)

6) how to connect it to thermistor (just plug or need to add some components?)

5) any other whole solution board ideas

thanks

Parents Reply Children
No Data