Hi,
I have a question regarding the absolute maximum TIN rating for the MAX233A.
According to the datasheet, the TIN rating for the MAX220, MAX222, MAX232A, MAX233A, MAX242, and MAX243 is listed as -0.3 V to (VCC - 0.3 V).
For the other devices—the MAX223, MAX230 ~ MAX241—the TIN rating is listed as -0.3 V to (VCC + 0.3 V).
I believe -0.3 V to (VCC + 0.3 V) is the standard, but is it correct that the MAX233A’s rating is -0.3 V to (VCC - 0.3 V)?
Best Regards,