MAX96717
Recommended for New Designs
The MAX96717 GMSLâ„¢ serializer receives video on an MIPI CSI-2 interface and outputs it on a GMSL2 serial link transceiver. Simultaneously, it sends and...
Datasheet
MAX96717 on Analog.com
MAX96716A
Recommended for New Designs
The MAX96716A converts dual GMSL2 serial inputs to MIPI CSI-2. It also transmits and receives control-channel data, enabling transmission of forward-path...
Datasheet
MAX96716A on Analog.com
Hello,
We are planning to use the MAX96716 with the MAX96717 to remotely connect a MIPI camera.
The camera has 2 lanes, 1 differential clock, 1 I2C interface, and 3 GPIOs.
Is it possible to use the two components in standalone mode without configuring them via the I2C interface?
Regards