I am working on a prototyping circuit which can be found in file “EquipLvlTest_Circuit_for_ADI_20260625.pdf”. The external MCU “Raspberry Pi Pico 2” is connected to “ADuM1250” side 1. The “ADuM1250” side 2 is connected to a multiboards environment with at least 3 EEPROMs and 1 master i2c controller. During the test, the waveform is captured as seen in the attachment. (Yellow Color Channel 1: ADuM1250 Side 1, Blue Color Channel 2: ADuM1250 Side 2). At Channel 2, the SDA logic LOW voltage is around 800mV. If include the noise, I have doubt that this ADuM1250 Side 2 I2C signal will give a clean signal to EEPROM Microchip 24LC64 and hence the EEPROM “ACK” is not response properly with a looked like floating signal in Channel 2 waveform.
From above info, can you advise is it I did not use ADuM1250 properly and caused the above issue?
EquipLvlTest_Circuit_for_ADI_20260625.pdf