What is the designed switching frequency of MAX3218 internal boost? Does it go into pulse-skipping mode at all? Our input voltage supply is +1.8V.
MAX3218
Production
The MAX3218 RS-232 transceiver is intended for battery-powered EIA/TIA-232E and V.28/V.24 communications interfaces that need two drivers and two receivers...
Datasheet
MAX3218 on Analog.com
What is the designed switching frequency of MAX3218 internal boost? Does it go into pulse-skipping mode at all? Our input voltage supply is +1.8V.
Geloism16 - Moved from Switches & Multiplexers to Interface and Isolation. Post date updated from Friday, June 19, 2026 4:10 PM UTC to Monday, June 22, 2026 5:15 AM UTC to reflect the move.
Hello,
My apologies for the delayed response. I have received your question, and I am looking into it. I will get back to you as soon as I can.
Thank you for your patience.
Best,
Shasta
Hello,
Thank you for your patience. The MAX3128 DC-DC operates in discontinuous conduction mode at low-load conditions. When VCC = 1.8V, at low-load currents, pulses may be as far as 200us apart (no load or very little load). The switching frequency increases to something closer to 200kHz (typ) under heavy loads.
Best,
Shasta